Tool/software:
Hi,
What is the maximum duty at the Buck-only operation?
Best regards,
Randy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
What is the maximum duty at the Buck-only operation?
Best regards,
Randy
Hello Randy,
Thanks for being patient with this. I will get back to you before the end of the week if that works for you.
Best Regards,
Ethan Galloway
Hello Randy,
The max duty cycle will depend on the switching frequency. The low side has a minimum ON time of 150ns. So, for example, the max duty cycle should be 97% at 200kHz. At 600kHz, the max duty cycle should be 91%.
If you need VAC=VOUT, you turn on bypass mode by setting EN_BYPASS=1. Bypass mode keeps the high side FETs always ON to pass current directly from VAC to VOUT.
Best Regards,
Ethan Galloway