This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: DCDC solution: input 30-130VDC, output 28V/42A.

Part Number: UCC28950
Other Parts Discussed in Thread: UCC28250

Tool/software:

My customer want to design a No-isolate DCDC, input voltage is 30-130VDC, output voltage is 28V and current is 42A.I run webench and suggest UCC2895x. But the customer thinks that the circuit of UCC28950 is too complex and hopes to find a simpler solution. Could you pls advise the suitable solution? Thanks.