This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600: app

Part Number: UCC28600


Tool/software:

If I want to add an on/off function in UCC28600, can I do it in the following ways as soon asUCC28740?

  • Hello,

    Your inquiry has been received and is under review.

    Regards, 

  • Hello,

    The OVP pin of this device is actually is use for ZCS detection as well as OVP.   I would not recommend using this pin to shut down the UCC28600.

    If you want to power down the UCC28600, I would recommend using a series pass regulator using an NPN transistor and resistors to pass and regulate voltage to VDD.  To turn-off the device you would then use a logic level FET to pull down on the NPN transistor to disable the UCC28600.  Please refer to the schematic below for details.

    Thank you for interest in Texas Instruments (TI) products.  If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

    Regards,