This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2217: Generating +12V/-12V out of +24V supply

Part Number: TLV2217

Tool/software:

For a new design we need a dual supply for an instrumentation opamp where we need a differential analog output between -10V and +10V.

So we need a double supply for the opamp. The operaring voltage for this instrumentation opamp is +9..+36V. So +15V/-15V would also be fine.

The total current consumption will be <10mA.

Do you have a device (we prefer low noise) that could perform this task or any other idea to generate dual supply out of +24V with low current consumption?

I had to fill in a device so I choosed the TLV2217 but we are not restricted to certain devices and I could not find a device with dual pos/neg output voltage.

Best regards Chris