Tool/software:
Hi Experts,
Good day. Seeking your assistance on this query from customer, to enlighten the confusion about the operation of the two-stage current protect "Over Current Protection" and "Short Circuit Protection" for the device TPS48111LQDGSRQ1.
In particular there are numerous references in the datasheet that the Short Circuit Protection uses the C_TMR timer in some way but also has an activation time of 1.2 or 4us. The exact function I want is, the Over Current Protection to use the timer and the Short Circuit protection to be very fast acting. Ideally the over current protection should auto retry, and the short protection should latch off. I don't understand what the purpose of the two protections levels is if they are forced to either both use the timer or both latch off.
Thank you.
Regards,
Archie A.