This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61020: 40kHz internal operation

Part Number: TPS61020


Tool/software:

Hi support team,

A customer reported that the audio signal of their finished product contained tone noise around 40kHz.
After investigating, we found that the power output from the "TPS61020" contained noise components of this frequency when observed with FFT.
The oscillation period of the TPS61020 is 600kHz, but when we placed a probe on the oscillation part (coil) and measured it with FFT, a large 40kHz tone (and 80kHz, which is thought to be a harmonic of it) was confirmed.
The PS pin is set to high and FPWM is used.

So, my questions are:
Are there any parts of the TPS61020's internal operation that operate periodically around 40kHz (1/15 of 600kHz)?
If there are, is there a way to prevent this from happening or to push it to a higher frequency?

I have attached the switching waveform of the coil.


There is some ringing, but it appears to be oscillating without any problems.
(However, there is a change point in the middle of the rise, and this appears to be fluctuating periodically.)

Regards,
Dice-K