This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25858-Q1: Value of Rcc1 and Rcc2

Part Number: TPS25858-Q1

Tool/software:

Hello,

Based on the schematics provided in the related question, my device is not detecting when I connect a device to the USB-C port. the Resistor (R8-R11) seem to be incorrect. I tested multiple values and nothing was working. So instead I changed to connection, as shown the R were connected to ground with a 1K resistor, but now i connected to PA_bus and PB_Bus with a 50.6K resistor. My device now detects a plugged device and provides 5V.  Could someone verify this is the correct function my design is supposed to work as a source not as sink. This is the reason I change the R value, the specifications does not clearly delineates the changes required and the EVM only shows Ra and Rd no Rp.

Thank you,

Jeison