Other Parts Discussed in Thread: TPS923653,
Tool/software:
I'm designing an LED driver, so I can dim an LED strip. My LED strip is 24V, and I was considering getting an LED power supply (just because they are easier to source, and are normally neater than other AC/DC converters, without any exposed leads or terminals, specially in the AC side of things).
I was wondering if a buck driver, like the TPS922053 would be valid in this scenario, where Vin is equal-ish to Vout (I don't plan to drive the LEDs to 100% light, so VOUT should be always lower than VIN). Would a buck/boost driver, like the TPS923653 be better suited for this scenario?
I was also thinking that, because I'm using a driver IC, would it be better if I remove the vias resistors from the LED strip? I don't have details about the LEDs themselves, so I don't exactly know what their Vf is, but I would assume that would lower the total voltage, and I don't really need the vias resistor if the driver is going to control the current, right?
Thanks!