Other Parts Discussed in Thread: BQ34Z100, GPCCHEM
Tool/software:
I am looking for an alternative fuel gauge to support a 10Ah battery pack. The current implementation use bq27441-G1 for a 7.8Ah battery pack. bq27441-G1 max battery capacity can be set is 8Ah. Most of the parts with system side implementation, single cell, I2C interface and impedence tracking fuel gauge for Li-Ion battery has max battery capacity can be set is 8Ah. The alternative with higher capacity available jump straight to 32Ah. Is there a reason?
Battery fuel gauges product selection | TI.com
What is my best alternative for a 10Ah Li-Ion battery with system side implementation, single cell, I2C interface and impedence tracking?
Is it possible to scale sense resistor of bq27441-G1 for 10Ah battery pack and scale reading accordingly in application. Will bq27441-G1 work with scaled sense resistor for 10Ah battery pack?