Other Parts Discussed in Thread: UCC28180, UCC24624
Tool/software:
HI ALL
We are currently designing a 1000W AC/DC system using a PFC UCC28180 + LLC UCC256604 without HV startup + SR UCC24624 configuration.
The design specification for Vout is 40V/25A.
Due to an initial issue with load extraction, we adjusted RISNS from 205 ohms to 68 ohms, which allowed us to successfully add a load of approximately 40V/1.5A (60W). However, when I attempted to increase the load to
2.5A (100W), the protection mode was triggered.

What aspects can be checked? The VFB voltage is approximately 3V under no-load conditions.
Reducing the resistance will lower the slope of VFB vs. Pin, is this approach correct?What slope (ratio) is correct?

sch_adp1000a_e20_20241109.pdf6153.UCC25660x_CALC_1.0_Noah.xlsx
How can I ensure that the VFB setting is correct and that it does not enter OCP, OLP, or burst mode?
Thanks f
Regards