Tool/software:
Hello!
I have a battery of two lithium-ion cells in series.
I want the RSOC zero level to be at 6.5V rather than at the end of the battery discharge (5V).
The battery went through the learning cycle with a minimum value of Term Voltage = 5V (as written in SLUA848–June 2018 3.6 Term Voltage).
Then it says: "After the learning cycle is completed, this value can be adjusted upwards if there is a need for the gauge to report 0% at a higher voltage".
Please tell me, do I need to change anything else in the settings besides the Term Voltage parameter in order to raise the RSOC zero level to 6.5V?
Does Design Capacity need to be changed?