Tool/software:
Hello,
How long does the UCD90160 take to boot up/configure itself when Vin = 3.3V is applied?
For our design, Rail#1 does not have a dependency and is supposed to start immediately after the UCD90160 chip is powered on and ready to go.
However on a board we see that the rail comes up after 20 ms, on another board it is 160 ms.
What could be reason for the two different start up times considering both boards have been programmed with the same UCD image?
Thanks