Tool/software:
Hello TI Team!
We would like to know if the TPS1685 can be used in parallel connection mode on a system with two separate power supplies that are designed to have the same output voltage (40V).
If so, do you have additional documentation about this use case?
We are looking into using a separate enable pin for each device, do you see a problem with this?.
Please see the diagram below:

Also, Is it possible to get the Altium files of the TPS1685EVM? We looked at the User's Guide, and the PCB layer plots are not available.
Thanks for your help!
Best Regards
-Diego Melendez Lopez