Other Parts Discussed in Thread: UCC28C42
Tool/software:
Hi,
I am looking into TI products to replace the FA5536P currently used in the product. The datasheet for FA5536P is here. The points to consider when selecting an IC are as follows:
-Current mode
-HV terminal available
-Fsw can be set to around 130kHz
-Dutymax=80%(typ)
I would like to select an IC with functions as close as possible to the FA5536P. In the TI product lineup, I think UCC28740, UCC28C42, etc. are similar products. Is my understanding correct?
I would also like to know if there are any similar or recommended model numbers compared to the above model numbers.
Thanks,
Conor