This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPIC6C596: EOS/EIPD in SER OUT

Part Number: TPIC6C596


Tool/software:

I have worked with TI FQE and submitted two QEM jobs: QEM-CCR-2410-00018 and QEM-CCR-2410-00019.  Both jobs are showing eos/eipd which we don’t understand how this happens if the SER OUT is clocked out of the device.  Can someone from the product line please contact me and I can share the schematic

  • Hi Irving,

    You can post the schematic here, or send it to me via private message if you do not want it posted on the public forum.

    I am working on pulling your quality reports... EOS usually occurs due to an overvoltage condition that violates the absolute maximum ratings of the device. Can you provide any additional information on the fault condition?

    Did the fault occur during final test or was this a return from the field?

    What was the test/operating condition during the failure? For example, does the failure occur on power cycle? Is there some stress test applied to the system during failure?

    Regards,

    Zach

  • Hi Zach,

    I sent you the schematic in a private msg 

  • Hi Irving,

    I will go ahead and close this thread for now. We will continue the conversation via private message.

    Thanks,

    Zach