Other Parts Discussed in Thread: BQ25798, , BQ25730, BQ25820, BQ25750, BQ24610
Tool/software:
Hello! As mentioned in the title, I developed a battery charger for sodium batteries using the BQ25798, based exactly on the BQ25798EVM PDF schematic switching at 1.5MHz. However, it looks like the chip is not capable of holding a constant current charging for 1S batteries higher than 3.5A and higher than 4.1A for 2/3/4S batteries. E.g I switch from 3.5 to 3.6A for 1S it starts making weird noises and the current drops to 0 and comes back
I'm using the same parts as for the EVM, and I tried to follow the pcb routing guidelines as closely as possible, yet it still struggles to hold anything above 4.1A. See the routing and schematic below:



I marked the input power with green and the output with purple. Is there something I am doing wrong with the routing? My input/output trace width is 0.6 mm (for BAT and VBUS pins) and the routes for the SW1 and SW2 pins are 0.3mm, with pcb density of 1oz at JLCPCB. Am I asking the SW lines for too much current? Could they be too narrow?
As for the layout example in the chip datasheet, it does seem to have a very solid ground plane around it, but I barely could get any ground plane around (on the top, since my layout is, from top to bottom, POWER, GND, SIGNAL, SIGNAL, GND, POWER) because of the high components density.


Or could it be from one of my settings in the TI CHARGER GUI? Also one thing that I noticed is that I can increase the current slowly as the battery gets charged. For example, my completely drained 2S would only draw up to 3.5A but when I charged it like 10% more it went up to 3.8A. As far as i know the charging current should not depend on the battery charge (and voltage) state, right?
These are my settings in the GUI: