Tool/software:
Hi team,
I have an additional question.
Q2
If the transformer primary winding is n1, the secondary winding is n2, and the transformer winding current change is ΔIP, then ΔILOUT/a1 should be derived from the formula n1 * ΔIP = n2 * ΔILOUT.
Why is there a coefficient of 1/2 multiplied to ΔILOUT/a1?
> This is to avoid running in voltage mode control.
> This is described in application note slua560 that can be found in the following link.
https://www.ti.com/lit/pdf/slua560
The AN states the following:
"If LMAG is too small the magnetizing current could cause the converter to operate in voltage mode control instead of peak-current mode control. This is because the magnetizing current is too large, it will act as a PWM ramp swamping out the current sense signal across RS."
Why does the voltage mode occur when the magnetizing current increases too much?
Also, why do we multiply ΔILOUT/a1 by 1/2? What is the basis for 1/2?
Why is VIN not VIN-2*VRDSON?
Q3
When LMAG is derived from the formula for the commutation current, I think LMAG is the sum of the transformer Lp and the resonant coil L1. Is that correct?
> Lmag is selected to avoid voltage mode control.
Isn't the magnetizing inductance LMAG the sum of the transformer's Lp and the resonant coil's Ll?