Other Parts Discussed in Thread: UCC25800
Tool/software:
On page no.31 of the datasheet of UCC25800-Q1, the value of parasitic capacitance at pin SW is mentioned as 170pF. Is this the parasitic output capacitance value across each of the two MOSFETs present inside the IC?? Or is it the combined total parasitic output capacitance of the two MOSFETs, thus implying that each MOSFET is having a parasitic output capacitance of 85pF??