Part Number: BQ40Z80
Tool/software:
HI, I have some questions.
I want to use BQ40Z80.
Trying to read data to SMBus by connecting MCU to BQ40Z80.
I want to read the data written below in real time. The application is a power tool(li-ion battery 5s2p 18v 8Ah).
- - cell voltage
- - charge/discharge current : 0~120A
- - cell temperature : -30 ~ 110 celsius
- - cycle counter
- - SoC : 0~100%(1% resolution)
- - SoH : 0~100%(1% resolution)
Question 1) Can I read all the data listed above in the BQ40Z80 configuration?
Question 2) Is it possible to adjust the scale factor and read the discharge current to 120A?