Part Number: TPS25983
Tool/software:
Hi,
I am writing to seek assistance regarding an issue I have encountered with the TPS25983xL e-fuse IC, which I am using for under-voltage (UV), over-voltage (OV), and current limiting protection.
Retry_dly= open
Nretry= short to gnd
Itimer= open
Rlim=300R =5A
Cdvdt=100nf
While testing the active current limiting function using e-loader , The e-fuse works as expected without a load connected. However, when I apply the load and reducing the resistance, the current exceed the 5A current limit and rising till it reach 5.85A and then the efuse shut down.
what can I do to to fix this issue ?
thank you,
Niv