I have designed a variable-output boost DC-DC converter (LM5158RTER) to step up 5 V to 40 V. However, after receiving the PCB, I noticed that the output is fixed at 4.98 V, even when adjusting the potentiometer in the feedback loop. I have attached the schematic for your reference. Could you please review it and let me know if you identify any issues?

One observation I made is that in the reference design, a resistor divider is used to feed the EN/UVLO pin, whereas I have directly connected this pin to VMAIN (5V). Additionally, the reference design includes a capacitor directly connected to GND in parallel with the current circuit (R197, C357) on the COMP pin. In contrast, I used a different configuration. Also, in the reference design, RT is connected directly to GND, while I have used a resistor (R196) in my design. Could you please advise if these differences could be the cause of the issue, or if there are other areas I should investigate?