This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25758: Can Two MOSFET with BQ25758 support bidirectional converter ?

Part Number: BQ25758


Tool/software:

hi,

A my account needs a bidirectional converter with below spec. Can BQ25758 setting in buck-only mode(only two MOSFETs(Q1 & Q2) are used) support reverse mode?

Forward way: From input to output; input voltage:18V---24V, output 8V/10A;

Reverse way: From output to Input: Output 8VOUT, Input: 12V/10A;