This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Customer get a requirement for the bi-direction for load switch for battery application.
Their spec requirement as below:
Input voltage: 0~5V;
Current above 200mA;
When EN is HIGH, need support current bidirection flow;
No QOD when enable is low;
Could you help recommend suitable solution?
Thanks and best regards,
Will
Hi Will,
TPS22916 have reverse current blocking.
I recommend TPS22991xN variant should be a good fit for the required application. Kindly check more the ti.com load switch page.
Best Regards,
Arush