The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74912-Q1: PSpice Transient Model example design does not simulate on PSpice for TI

Part Number: LM74912-Q1
Other Parts Discussed in Thread: LM74912

Tool/software:

I've downloaded LM74912-Q1 PSpice Transient model (snom786.zip) and I'm trying to simulate the example design included with the model (LM74912-Q1 STARTUP SIMULATION). The tool version I'm using is  following "PSpice_TI 23.1-2024 S001 Winfows SPB 64-bit Edition"

When I'm running the simulation included with example schematic (SCHEMATIC1-StartUp) following errors are present in StartUp.out.1

--

INFO(ORPSIM-15423): Unable to find index file nom.ind for library file nom.lib.

INFO(ORPSIM-15422): Making new index file nom.ind for library file nom.lib.

.lib "filtsub.lib" ; Filter biquad stages and LC ladder branches

ERROR(ORPSIM-15116): Unable to find library file filtsub.lib.

Index has 74 entries from 2 file(s).

ERROR(ORPSIM-15107): Unable to make index for library file C:\Users\tero\Downloads\snom786\nom.lib.

ERROR(ORPSIM-15460): Subcircuit BUK7Y4R8-60E is undefined

ERROR(ORPSIM-15460): Subcircuit BUK7Y4R8-60E is undefined

ERROR(ORPSIM-15460): Subcircuit LM74912_Q is undefined

--

Is the model and example compatible with PSpice for TI? 

How to solve this problem?