This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC39002: How to Integrate UCC39002 with a Power Supply Lacking Remote Sense Inputs

Part Number: UCC39002
Other Parts Discussed in Thread: UCC29002

Tool/software:

I am designing a power supply system that incorporates the UCC39002 load share controller. My power supply currently uses a standard feedback topology with a single resistor divider network connected to the output voltage (Vout) for regulation. It does not have dedicated remote-sense inputs (positive and negative sense lines) to measure voltage directly at the load terminals.

The UCC39002 documentation specifies that the power supply must support remote sensing to properly implement load sharing. Given that my power supply lacks remote-sense inputs, I have the following questions:

  1. How can I adapt my existing feedback network to work with the UCC39002?

    • Can I derive the equivalent of a remote-sense signal by modifying the feedback circuit?
    • Would it be possible to add external sense lines or simulate them with minimal changes to the design?
  2. Is there a recommended circuit modification to couple the UCC39002 with a power supply that regulates locally using a resistor divider?

  3. What challenges or limitations should I expect when using the UCC39002 in this scenario without traditional remote-sense lines?

Any guidance, application notes, or design examples for adapting the UCC39002 in this type of setup would be greatly appreciated.

  • Hello Miguel, 

    If your power supply does not have a remote-sense input, you have to create one.  This is done by splitting the upper resistor (Rvs1) of the feedback divider network into two resistances.  The ADJ signal attaches to the tap between these two resistors. 
    The top one becomes the Radj resistor and has a relatively low value as designed with the UCC39002 calculator tool.  The bottom one becomes the value Rvs1-Radj.  
    Usually, Rvs1 is so much >>Radj that it is easier to simply add Radj in series with the existing Rvs1. 

    I'm sorry I am unaware of any application notes that explicitly address this issue.  

    Conceptually, this situation can be considered to be adding Radj in parallel with an infinite Rsense resistance (not 0 ohm).
    The UCC29002 Excel tool accommodates this situation by recommending to set the value of Rsense to 100kR for cases where there is no remote sense. 
    https://dr-download.ti.com/design-tools-simulation/calculation-tool/MD-GtQkXDHgDE/1.1/UCC29002_Design_Calculator.xlsx

    1 & 2 are the same question and are answered above. 
    3: The only challenge is to gain access to the top resistor of the existing feedback divider network and insert Radj between it and the Vout rail.  

    Regards,
    Ulrich