Tool/software:
I have a question about the formulas in Fig. 1 and 2 on the following website.
Understanding MOSFET Data Sheets, Part 3 - Continuous Current Ratings
https://www.ti.com/document-viewer/lit/html/SSZTCP0
Formula Fig. 1
①When calculating MaxPDiss, if the ambient temperature changes, will the 25°C in the formula be that temperature⑤?
②If Rθjc in the formula changes to Rθja, can the same formula be used for calculation?
Formula Fig. 2
③If I substitute the MaxPDiss calculated above into MaxPDiss in this formula to calculate ID, will it be the ID at that temperature ⑤?
④Is it correct to understand that the rated power consumption and rated current of a MOSFET change (decreases) depending on the temperature?