Tool/software:
Hi Team,
We recently purchased a couple of eval boards(TPS7A4701EVM-094) for TPS7A4701 device from Mouser. As per the datasheet the device should be able to source up to 1A of current but unfortunately even with a simple resistive load of 10 mA, the device seems to go into shutdown mode and delivers only 0V. If the jumper J8 is left open the output voltage is the same as the input voltage, this behavior is different from what is documented in the datasheet.
The ramp-up and ramp-down time seems to be too long even with no load connected. Is there a way to calculate the capacitor values to reduce the ramp-up and ramp-down time?
We have based our designs based on this device, if this is not resolved in the next couple of days we will be forced to redesign with a different LDO. Kindly support at the earliest.
Regards,
Sridhar C
Ciphor