This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25660: UCC256601

Part Number: UCC25660


Tool/software:

LLC power

  • Hi Pertti,

    Can you clarify your question? 

    Thank you,

    John

  • Hi John,

    We have now developed an LLC power supply (input 395V; output 24V 300W) using the OnSemi FSFR2100 controller and Magnetica transformer 1860.0160.
    The OnSemi FSFR2100 is now EOL, and we need to redesign with a different controller with minimal changes.
    I used TI WEBENCH, which suggests using the UCC256601 controller, but it does not recommend any ready-made transformers.
    TI has an EVA board UCC25660EVM-064, but its output is only 12V, and we need 24V.
    Is it possible to modify this board to achieve a 24V output, or do you have another EVA board with the UCC256601 that has a 24V output?
    Can I use that Magnetica transformer with UCC256601 controller?
    Or, what would be your recommendation for achieving the best result?

  • Hi Pertti,

    PMP23463 is really close to what you are looking for. This could be your best starting point. 

    I hope this answers your question.

  • Hi John,

    That looks good. Where can I buy those?

    BR, Pertti

  • Hi Pertti,

    Our reference designs are not normally available for sale, but we do provide everything you need to start you own design. Do you have a local sales contact who can help you?