Tool/software:
Hi,
I want to converter my battery voltage which varies from 18V to 25.2 V to dual polarity voltages (adjustable) from +/- 25V to +/- 48V with output current of at least 5A.
Input Voltage: 18 to 30V DC
Output 1: 25 to 48 V
Output 2: -25V to - 48 V
Output current adjustable: 5A to 10A
Size: 70m x 50 mm x 25 mm
Please let me know which parts would be very suitable for it.