Other Parts Discussed in Thread: LMG1210
Tool/software:
Hi, I found out that the C-boot is not charging up to 5V at every switching cycle. I'm attaching the scope traces of the HB-HS w.r.t other signals.
The board was supplied with only Vin = 12V drawing about 1.8W.
How can we resolve this?
I bought the EVM through Digi-key.
In the screenshot, C1 = HB-HS, C2 = Vbus 0V, C3 = LO, C4 = PWM(TP9)
Thanks.

Yellow = HB-HS, Red = HO, Blue = LO, Green = PWM @TP9
A zoom in view of above.
Yellow = HO, Red = Vbus 24V, Blue = LO, Green = PWM @TP9