This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Aki,
We unfortunately do not have a 4.5V device for the LM8364, but we do have the TLV840NADL46DBVR, this device is pin-to-pin with the LM8364, but it has a 4.6V threshold compared to the 4.5V of the LM8364.
If 4.5V is a hard requirement, we have the TPS3840DL45DBVR, this one is "conditional Pin-to-Pin" with LM8364, with 4.5V threshold.
Conditional pin-to-pin means as long as pin 4 and pin 5 are floating, the devices are pin-to-pin
Jesse