Other Parts Discussed in Thread: TPS61169,
Tool/software:
Hi,
Working on a customer design, consumer electronics, with the need to power a LCD display backlight. Display has 6 LEDs connected in parallel, resulting in Vforward of 3.3 +/- 0.2V and Iforward of max 120mA spec on the backlight. Goal is to be able to power the driver directly from the product battery supply, which is 2x 1.5V alkaline AA-batteries in series for a nominal 3V supply.
First prototype used a TPS61169 driver powered from a regulated 3.3V rail, but this didn't work well since the lowest brightness achievable is higher than wanted. So we need to select another driver and I'm looking for advice.
Can TPS61043 be used in this application? I suspect this means I need to limit the LED current to 60mA since "Maximum LED switch current" through Q2 is limited to 60mA ? Are there better driver alternatives? I'd like to remove the backlight driver from the regulated 3.3V rail as well since it causes more strain on this 3.3V rail than wanted.
This is a custom display, so we have the option as well to ask the display manufacturer to connect the total of 6 backlight LEDs in series instead, or maybe a combination of two string of 3 LEDs in series for a 9.9V +/- 0.6V / 60mA specification if that makes the driver selection easier?
Thanks
Daniel