Part Number: BQ25798
Other Parts Discussed in Thread: BQ25792
Tool/software:
Hello,
I am working on a project that involves interfacing the BQ25798 battery charger IC via the I2C protocol. My goal is to configure the IC for battery management tasks such as setting input current limits, charge voltage/current, and monitoring battery parameters like voltage and current. Additionally, I aim to handle fault conditions such as over-voltage and over-temperature. The communication interface will operate at 400 kHz (Fast Mode).
I am looking for any existing driver code, libraries, or sample applications for the BQ25798 to streamline development. I have reviewed the datasheet and register map and explored the TI Resource Explorer and GitHub for relevant resources but could not locate suitable examples. I would appreciate guidance on specific initialization sequences, register-based configurations, or interrupt handling for this IC. If pre-existing libraries or application notes are available, they would be greatly beneficial.
Thank you for your assistance and support!