This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: GPCRB status 06

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: GPCRB, GPCRA0

Tool/software:

Hello,

I want to do the GPCRB. I export gg.csv, it is 0E of the Update Status in this gg.csv.

When I get TI report (gg_out.csv / chemdat12_IDxxxx) from TI GPCRB tool. it is 06 of the Update Status in this gg_out.csv.

I have one question, may I need to do one cycle (charge->relex->dsg), let it 06 to 0E. And then export golden file (srec and gg file).

Or It is okay of the 06 and export golden file (srec and gg file) directly.

Thanks,

Mulin

  • Hello,

    There is something wrong with my GPCRB-report. Why does the QMAX CEll change from 6614 to 17799? 

    Please help confirm where the problem.

    4S2P to make GPCRB.zip     4S2P to make GPCRB-report.zip

    Thanks

    Mulin

  • Hi Mulin,

    In the low temperature data sent, there is a significant drop in the voltage during the discharge. Can you please confirm whether a cell got disconnected at this time or if this is repeatable:

    Regards,

    Anthony

  • Hi Anthony,

    Q1:

    Do you mean this point, it seem to me that it is correctly.

    Refer to cell spec of discharge characteristics of NCR18650GA at-20℃,0.2C,1.0C

    My SPEC, 4S2P 18650GA, DSG: 5A (system current), Ta: -20 degree C

    Q2:

    I want to do the GPCRB. I export gg.csv, it is 0E of the Update Status in this gg.csv.

    When I get TI report (gg_out.csv / chemdat12_IDxxxx) from TI GPCRB tool. it is 06 of the Update Status in this gg_out.csv.

    I have one question, may I need to do one cycle (charge->relex->dsg), let it 06 to 0E. And then export golden file (srec and gg file).

    Or It is okay of the 06 and export golden file (srec and gg file) directly.

    Thanks,

    Mulin

  • Hi Mulin,

    Regarding the Qmax change, this should not happen since the Qmax Delta value should limit the maximum change in Qmax per update (in your .gg it is set to 15%). If the Qmax values are changed back to the learning cycle values and ran through the application typical load, how large is the change in Qmax?

    I have one question, may I need to do one cycle (charge->relex->dsg), let it 06 to 0E. And then export golden file (srec and gg file).

    Or It is okay of the 06 and export golden file (srec and gg file) directly.

    I believe both options are sufficient. When the gauge is deployed in application, the learning status will update to 0E when a field update occurs, so the .srec can be exported with a learning status of 06.

    Regards,

    Anthony

  • Hi Anthony,

    Regarding the Qmax change, this should not happen since the Qmax Delta value should limit the maximum change in Qmax per update (in your .gg it is set to 15%). If the Qmax values are changed back to the learning cycle values and ran through the application typical load, how large is the change in Qmax?

    To make GPCRA0 and export the gg.csv file, please refer to the below attached, Qmax is 6614.

    Because my customer had issue at low temp., want to make GPCRB.

    6472.gg.csv

     

    I have one question, may I need to do one cycle (charge->relex->dsg), let it 06 to 0E. And then export golden file (srec and gg file).

    Or It is okay of the 06 and export golden file (srec and gg file) directly.

    I believe both options are sufficient. When the gauge is deployed in application, the learning status will update to 0E when a field update occurs, so the .srec can be exported with a learning status of 06.

    Thanks.

  • Hello,

    This week is a holiday in America, we will get back to you next week.

    Regards,

    TI BGP Team

  • 嗨安東尼,

    Regarding the Qmax change, this should not happen since the Qmax Delta value should limit the maximum change in Qmax per update (in your .gg it is set to 15%). If the Qmax values are changed back to the learning cycle values and ran through the application typical load, how large is the change in Qmax?

    1.我重新測試了GPCRB,Qmax正常,tks。

    謝謝,

    穆林