Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
Hi,I applied the bq40z50-r2 device to a 2S1P battery pack, extracted the chemical ID, and after completing the learning, I was able to accurately estimate the battery level and full charge capacity accuracy, and used it in practical application scenarios without any problems. But when I used it in bulk, I found that two new batteries suddenly had their FCC drop from 2100mAh to 900mAh during discharge, and their SOC suddenly changed from 55% to 0. From the logs obtained from our application device, we did not find that the battery cell voltage had reached the cut-off voltage. I know that when the cell voltage reaches the cut-off voltage, there will be a SOC jump to 0, but obviously it is not the reason. Due to the low probability of occurrence, Battery Management Studio cannot be used to collect logs. Therefore, please provide some possible reasons for this abnormal situation. thank you