Tool/software:
Hi Team,
We are using UCC14141-Q1 for gate driver power supply with +15V and -9V.
On power-up with EN and PG pins 5V & Vin as 12V, we are not able to get the output across any of Vdd to Vee or Vdd to COM or COM to Vee.
RLIM value is 1k ohm.
Vdd to COM capacitor is 10uF.
COM to Vee capacitor is also 10uF.
What could be the issue?