Tool/software:
Hello,
I am using the BQ79718V AFE and i use 15 cells of 3.2V each which is 48V.
I have some questions:
1. In active mode the LDOIN pin i consumes 10mA, why is that? i saw that in the datasheet it says 6mA
2. Is it ok to use external power supply (like buck) of 6V to the LDOIN pin to reduce the power consumption of the external fet? because if i use the external fet the power consumption is 48V*10mA, and if i will use another power supply the power consumption will be 6V*10mA
3. i want to turn off the 6V power supply to the LDOIN in shutdown mode. Is it ok to do that? Is it ok to turn off the LDOIN voltage and still apply voltages to BAT, CB15,VC15, etc..?
4. In the case of using external 6V supply, what to do with the NPNB pin?
Thank you
Maor Matityahu