This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65051-Q1: Any IC from TI similar to TPS65051 (ie with both DC-DC and LDO in it)

Part Number: TPS65051-Q1

Tool/software:

Hello,

Are there any power management ICs similar to TPS65051 from TI, ie an IC which has both DC-DC and LDO. And approx 2A rating for the DC-DC.

That is, an IC that supports:
1 or 2 DC-DC converters (with 2A output rating). Needs on the board are: 5V to 3.3V - with 1.5A requirements ; 5V to 3.8V approx A (even a 5V to 2.5V can be put on the DC-DC)
And 1 or 2 LDOs, which will take outputs of one of the above DC-DC.

A device that will help reduce board area would be a great advantage. eg: two DC-DC and two LDOs would also be ideal.

Attempt is to find a device closely similar to TPS65051 .