Tool/software:
The datasheet for this part seems to indicate that the max power point occurs when:
-the Ics produces a peak voltage of 770mV (Vcst(max) on the datasheet) AND
-when the frequency is at 105kHz
Although the design worksheet I downloaded seems to indicate that 80kHz is the max frequency.
I filled out the design worksheet, but It's not clear whether my design will yield the desired output, or if there are any other problems.
There are a couple of places where the text in the design worksheet is red, but I don't see any values that are specifically concerning.
Can someone double check me on this and tell me if the design worksheet is indicating a problem?
sluc652b.xlsx
Thanks,
Mike