Other Parts Discussed in Thread: TMS570LS1224, BQ79616, USB2ANY
Tool/software:
The architecture is based on the TMS570LS1224 as the MCU, communicating with the BQ79600. I used the SPI sample code provided officially for testing but found that I couldn’t successfully wake up the BQ79600.
- J10: 1-2
- J11: 1-2
- J12: 2-3
- J6: 1-2
- J1: 2-3
- J3: 2-3
The power supply is 5V, and the input is p Post ulled from the MCU side.