This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: About TVS and IEC 61000-4-2 test question.

Part Number: TPS1663

Tool/software:

Hi team,

The electrostatic curve time of IEC 61000-4-2 Contact discharge will be as short as ns. At the same time, I do not want to cut off the load power when the input side TVS is activated,

otherwise, it will not comply with the specification.
So I would like to ask if you have done similar tests or have any suggestions for the combination of external parts of the circuit? Thanks