This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1685EVM: How to set up the EVM if I would like to use resistors as load?

Part Number: TPS1685EVM

Tool/software:

Hi Team

I would like to using resistors as load for TPS1685EVM test, but the output can not go well when the current is over 600 mA. On another hand, the test is OK if I use Electronic Load as load to test.

The fail situation is shown as follow. (Red signal is DVDT, Yellow is Output, Blue is Input and Green is Current.) 

Thanks a lot

Best wish

Steven