Other Parts Discussed in Thread: UCC28951, UCC28950, UCC2808A-2, LM25037
Tool/software:
Hello,
I am trying to design a 1 kW DC/DC converter whose output will be used for a sinusoidal pwm full-bridge inverter.
My specs for the converter stage:
- Input Voltage: 24 V DC (2 series lead-acid battery each is 9Ah)
- Output Voltage: 400 V DC
- Output Current: 2.5 A max.
- Switching frequency (each channel): 100 kHz
- Output Rectification stage is going to be full-bridge rectification.
For this kind of design, I need to choose a controller such as UCC28251. But, I am not sure if this IC will be able to meet those requirements. Can you please confirm?
If it cannot, can you please advise me another IC that can handle it.
Thanks in advance
Sincerely
Can