This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: How to connect a charger and current sensor

Part Number: BQ77915

Tool/software:

I'm using the BQ7791500 with a 0.025ohm resistor. 

I'm unsure as to the maximum current the IC can handle in a short circuit discharge. 

I don't understand how to connect my charger IC to the BQ77915. I was trying to do something like this : 

but i'm not convinced it will interrupt my charge/discharge in case of fault condition. 

Thank you !

  • Hi Alyson,

    You can refer to the recommended maximum ratings of the SRP and SRN pins to determine what current the device is capable of handling.

    That is the recommended way to connect a charger. The CHG FET will correctly block the charging current from flowing.

    Regards,

    Max Verboncoeur