Other Parts Discussed in Thread: TPS5450
Tool/software:
We are using tps2595 for undervoltage, overvoltage and short circuit protection for our device. Undervoltage and overvoltage protections are working fine but the issue we are facing is with short circuit protection. When we shorted 5V and GND pins together then we observed that area around TPS5450DDAR buck converter got very hot, we had to remove the short circuit. We are suspecting that short circuit protection is not working in our system. Because if short circuit triggers then there should be complete power cut from the system and no component should get hot or damaged. Schema 2024-10-28.pdfI am attaching schematic for reference. Your help will be appreciated.