Other Parts Discussed in Thread: LMZM23601, TLVM23615,
Tool/software:
Hi support team,
I am considering changing from LMZM23601 to TPSM33615 or TLVM23615.
I will use it under the following conditions.
Vin: 24V
Vout: 5V
Iout: 0.6A
The inductor has been reduced from 10μH to 2.2μH.
What are the conditions for switching to PFM?
Is it when the inductor valley current is less than 0A?
Regards,
Dice-K