Other Parts Discussed in Thread: LM5180, LM25184
Tool/software:
Hi Sir
I want to design a power supply using LM5185 IC which will have two outputs. Will you please suggest suitable transformer for this application. Please look into this
IC: LM5185
Input Voltage (min) 10 Volts
Input Voltage (nominal) 24 Volts
Output 1: 5 Volts 1 A DC
Output 2: 5 Volts 200 mA DC
Isolation: Yes
Operating Temperature: - 40 °C to + 85 °C
Thanks & Regards