This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM83102: DC DC Boost converter

Part Number: TPSM83102

Tool/software:

I am looking for DC DC Boost converter.

The output we need 1 A on +5V and 1 A on -5 V.


The input voltage is 2.75 V but the current is up to 6 A can be drawn from the supply.

At the moment no preference for cost and size but should be possible to place and add in the PCB design.