This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR51430: LMR51430 controlled by digital potmeter

Part Number: LMR51430

Tool/software:

I would like to control my LMR51430 with a digital potentiometer
for example a mcp4132 or mcp41010 (1mA max potentiometer current)
output voltage is adjustable between 5 and 20V max current 3A input voltage 24V
what values ​​are needed for the resistors and coil.
  • Hello,

    Please refer to the Applications Section of the device datasheet for recommendations on properly sizing the inductor and FB resistors.

    For the inductor, optimize the value for your worst-case operating conditions.

    Best regards,

    Ridge