Tool/software:
Dear TI engineers,
I would like to know how much voltage can be output when Vin is 10.8V in the worst case consideing deviation.
In the section 6.6 of dataseet, I can see that Max duty cycle is defined as 99%. But 99% is only typical value and there is no description on Min value.
I think it can be calculated by using the maximum value of tMIN_OFF and the minimum value of tMAX_ON if both value have independent deviation(in the case if both value have proportional relation, the worst ratio of both value can be used).
Best regards,
YTK